A customer needs a boat hoist system in order to lift boats out of water for maintenance purposes. They would like a wireless solution in order to monitor the forces being applied through the hoist system.
A customer needs a boat hoist system in order to lift boats out of water for maintenance purposes. They would like a wireless solution in order to monitor the forces being applied through the hoist system.
Interface Solution
Interface suggests using multiple WTSSHK-B Wireless Crosby™ Bow Load Shackles at the pick up points of the hoist mechanism. Data results of the individual loading points and total weight can be transmitted wirelessly to the WTS-BS-4 Industrial USB Base Station when connected to a PC or laptop with supplied Log100 software.
Results
Interface’s wireless system and solution successfully measured the weight of the boat and ensured it would be safely lifted out of the water.
Materials
WTSSHK-B Wireless Crosby™ Bow Load Shackles
WTS-BS-4 Industrial USB Base Station with supplied Log100 software
WTS-HK-S Next-Generation Wireless Handheld
Customer PC or Laptop
How it Works
Multiple WTSSHK-B Wireless Crosby™ Bow Load Shackles are installed to the boat hoist mechanism.
The boat is lifted out of the water, and the force measurements are wirelessly transmitted to the WTS-BS-4 Industrial USB Base Station. The customer can measure the individual loading points and total weight.
When connected to a PC or laptop, force data can be logged and graphed with Log100 supplied software. Loads can also be seen using the WTS-HK-S Next-Generation Wireless Handheld.